Corcom | TE Connectivity
TE Connectivity’s Corcom is a leader in RFI technology. As every electrical or electronic device has connections that are a potential source for electromagnetic or radio frequency interference (EMI/RFI), the TE Connectivity Corcom line offers over 70 filter series that provide solutions for to solve EMI or RFI signal issues. The Corcom product line includes telecom and Ethernet connectors, EMI / RFI suppressors and ferrites, feed-thru capacitors, frequency control filters, as well as power line filters.
For over 60 years, Corcom has been providing solutions to leading telecommunications, computer, industrial and medical companies worldwide.
View the TE Connectivity Manufacturer page.
TE Connectivity, TE Connectivity (logo), and TE are trademarks owned or licensed by the TE Connectivity Ltd. family of companies.

TE Connectivity (TE) adds more range to the FB series product line with new part numbers designated with FBL. FBL is part of the FB series and is targeted toward applications that need standard EMI performance levels. LED Drivers have different levels of integrated filtering but when connected to a load the filtering may not be enough to attenuate the conducted emissions. The FB series offers standard performance filtering with the FBL designated filters and high performance with the FB designated filters. In addition, lighting applications can reach higher currents and the 10 and 20A versions of the FBL products will satisfy those types of applications. Designed to work with lighting applications that require 300 VAC.
IH Series Medical Filters
TE Connectivity introduces the Corcom IEC inlet RFI filter IH series to suppress electromagnetic interference (EMI) conducted in equipment used in medical environments requiring C18 ungrounded inlets. These RFI filters are also suitable for use in laboratory, test and measurement equipment. TE Connectivity Corcom IEC Inlet RFI Filter IH Series
TE’s Corcom filter IH series enables medical equipment manufacturers to comply with the international standard IEC 60601-1, which sets specific safety requirements to equipment designed for home use. These filters also adhere to the stringent safety standards and are classified as meeting 2MOPP requirements (two means of patient protection, also referred to as double insulated). TE’s RFI filters help attenuate EMI in the frequency range between 150 KHz and 300 MHz, as required by FCC Part 15 and EN55011 and EN 55022 standards.
The filtered inlets integrate a notch into the inlet to make it compatible with V-Lock locking cords. This feature helps minimize accidental disconnection of the power cord from medical device. The TE Corcom filter IH series is available with snap-in mounting for quick installation or with flanges for extra-rigid mounting.
Feature & Benefits:
- Meet IEC 60601 leakage current requirement through an IEC 60601 compliant filter
- Help eliminate accidental power disconnection of equipment through V-Lock cords
- Help save installation time through an integrated cord lock that installs and operates without additional parts or tools
- Protect against radiated emissions through a shielded filter assembly
- Support in minimizing equipment size with a small, compact filter