1. Home
  2. /
  3. Blog
  4. /
  5. Press Release
  6. /
  7. Heilind Expands Cable Management Portfolio with HellermannTyton In-Line...
HellermannTyton

Heilind Expands Cable Management Portfolio with HellermannTyton In-Line Ratchet P-Clamp

WILMINGTON, Mass. (PRWEB) June 30, 2021 ― Heilind Electronics, a premier distributor of electronic components worldwide and an authorized distributor for HellermannTyton, has introduced the in-line Ratchet P-Clamp to its portfolio of cable management products. Engineered for heavy-duty applications, it creatively solves wire bundling challenges in OEM, automotive and solar installations.

The HellermannTyton Ratchet P-Clamp features an adjustable ratchet clamp mechanism and is offered in five sizes with multiple mounting options. The innovative design helps to reduce parts and inventory costs while saving the time required for wire harness and cable installation and maintenance.

The construction of the Ratchet P-Clamp opens the way to a more efficient division of pre- and final assembly. Simply position and fix the opened Ratchet P-Clamp first, then fasten the bundle — or conversely, apply the clamp to the bundle first, then fasten it to the mounting point. The adjustable clamp is easy to close by hand to the precise diameter required. There is no slack and the rifling on the inside of the clamp automatically centers the bundle and minimizes the risk of pinching.

The robust Ratchet P-Clamp can be used at operating temperatures between minus 40 degrees Celsius and plus 125 degrees Celsius (up to 150 degrees Celsius for 240 hours). The polyamide 6.6 plastic used is high impact-modified, as well as heat and UV stabilized. The zinc-plated stainless steel mounting plate is suitable for high torque.

Visit HellermannTyton’s Ratchet P-Clamps page for more information.

About Heilind Electronics
Heilind Electronics, Inc. is one of the world’s leading distributors of connectors, relays, sensors, switches, antennas, thermal management and circuit protection products, terminal blocks, wire and cable, wiring accessories and insulation and identification products. Founded in 1974, Heilind has locations throughout the U.S., Canada, Mexico, Brazil, Germany, Singapore, Hong Kong and China.

About HellermannTyton
HellermannTyton is a leading global manufacturer of systems and solutions which help world-class customers better manage and identify wire, cable and components. Located in over 34 countries, HellermannTyton offers an integrated approach in the design, manufacturing and delivery of its products, which results in higher quality and lower costs for customers.

View the original press release

Share this page